STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! include <new>

../Middlewares/ST/touchgfx/framework/include/mvp/MVPApplication.hpp:22:10: fatal error: new: No such file or directory how to solved this? cubeide 2.0.0 GNU  Tools for STM32 (14.3 rel1)

Resolved! updateTime and updateDate touchGFX

I am using STM32H750B-DK  (DK32H750BSAT1). Following st tutorial in:https://www.youtube.com/watch?v=dx7xHRH9YXg The project built and ran successfuly on the board. Unfortunately upon implemeentig the updateDate on a textArea the update stopped comple...

ksale.1 by Senior II
  • 761 Views
  • 5 replies
  • 2 kudos

Resolved! TouchGFX + Free RTOS TImer and Thread

Hello. I'm using STM32H747XI with touchgfx designer 4.24.2 and Free RTOS 10.3.1. In this RTOS I setup some threads(with osPriorityNormal 24) and a Periodic Timer at 400ms.   I notice that when I start this thread void threadEntryPoint() { // Puli...

Resolved! Duplicate Items when using Scroll wheel

Setup:TouchGFX v4.23.0STM32H747Scroll wheel with selected item template Issue:I dynamically set the number of items in the scroll wheel using the function setNumberOfItems() so in the TouchGFX designer I set the Number of Items to 0.  As an example, ...

brymat by Associate II
  • 4003 Views
  • 6 replies
  • 0 kudos