cancel
Showing results for 
Search instead for 
Did you mean: 

LCD flicker following new FW being flashed

Hi all,

I have a screen with an RGB interface (Focus LCD E35KA-FW1000-N) that's being driven by an STM32H747 with the framebuffer in external RAM (over FMC). I'm presently using a double framebuffer strategy, but this same behaviour occurs when I used single.

After flashing new FW, the screen flickers quite badly, and then over a few minutes it settles down and I have a beautiful screen with immediate transitions and no flickering. While it's flickering, you'll see the previous image it was displaying in the background. I'm not too worried about this, it disappears once the flicker is gone.

What could be causing this? 

I can't share the project (under NDA), but I'll gladly answer any relevant questions that can help someone help me solve this. Thanks in advance,

Julia

8 REPLIES 8
GaetanGodart
ST Employee

Hello @jchernus-fikst ,

 

Can you share your setup parameter for the screen?
Perhaps your LTDC configurations?

This datasheet : https://www.hpinfotech.ro/ILI9488.pdf tells you some timings to follow :

GaetanGodart_0-1741861005182.png

 

Is the horizontal synchronization, vertical back porch and DOTCLK Frequency correctly setup?

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

Hey @GaetanGodart,

Thanks for responding. Here is the information you asked for:

jchernusfikst_0-1741889187242.png

The values for the first two sections, "Synchronization for Width" and "Synchronization for Height" were provided by Focus LCD. The Signal Polarity I worked out myself.

The DOTCLK frequency is set to 12,307692MHz, which is just above 389 x 507 x 62 = 12.227.826

I believe these all to be within the acceptable bounds. Like I mentioned in my last post - the screen performs wonderfully a few minutes after flashing and has no artifacts during a power cycle. It only happens while flashing.

My problem with this behaviour is that it sticks around for several minutes and looks unprofessional, so I need to fix this before we get this product into the hands of Beta customers. 

Thanks for your help!

Julia

 

Some more settings, in case they're relevant - to avoid going back and forth.

More from LTDC

jchernusfikst_3-1741889621899.png

jchernusfikst_2-1741889610770.png

TouchGFX

jchernusfikst_4-1741889644682.png

DMA2D

jchernusfikst_5-1741889667114.png

Thanks again!

Julia

@GaetanGodart any suggestions for how to proceed? Thanks!

Hello @jchernus-fikst ,



We did not see anything wrong with your implementation.

Maybe the flashing uses some of the pins used for the init.
Can you try to reset your screen after flashing (at the beginning of your application) thanks to the reset signa,l RSX pin, pin 36.

 

You are un RGB mode right, not MCU mode? (I guess it wouldn't work if in MCU mode)

Could you try to increase a bit your DOTCLK ?

Could you try to run your display with the values in the example?

GaetanGodart_0-1742554334681.png

 

Once that is done you can check your framerate by checking VSYNC (if using TouchGFX, you can just call a pin VSYNC_FREQ to get it).

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

Hello @jchernus-fikst ,

 

Just checking in, did you manage to fix your display flickering?

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

Hi Gaetan,

No, every time we flash the unit with new FW, it flashes back at us for ~2 minutes. We decided we could live with it through some user-research and early prototypes, but now we're moving onto Beta and I need to get it fixed.

To answer your previous questions,

I am resetting the screen (hard & soft) on every initialization.

I tried increasing the DOTCLK and it made no difference, I'm within the range you shared, 10-20MHz.

We are operating at a VSYNC_FREQ of 16ms, i.e. ~60fps.

 

Thank you,

Julia

Does flickering occur in the non-TouchGFX cases, ie you just painting a static (or different) images from the frame buffer?

Say a more stand-alone example like the PicturesFromSD, etc that come in the Cube repos for DISCO, DK and EVAL boards?

Not sure what TouchGFX would be doing in the minutes after an Internal/External memory update that wouldn't be occurring at every other power cycle.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..