STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Making an infinitely long scroll list in Touchgfx

I would like to display the received SPI data on a scroll list container from TouchGFX. But the thing is, data are coming in at high rate, around 10,000 times in a second and each of these data need to be display on reach row of the table.Is there a ...

inf.PNG

Enabling double framebuffer on DSI displays

Hello TouchGFX Community!This post is not a question, it's just a little tutorial on how to use double framebuffer strategy on DSI displays. We saw that this is something a lot of us want to do to improve performance, so here's how you can do it :)No...

0693W00000QL7D3QAL.png 0693W00000QL7E1QAL.png

Lagging

I upload code to my custom board and it works fine until I open custom container and it starts lagging (with others custom containers in that screen does not lagging) in other screens also the same problem. I've tried to comment code in this custom c...

heyo by Senior
  • 1186 Views
  • 0 replies
  • 0 kudos

toughgfx change screen from button virtual function?

Hi all,I want to change from firstScreen to secondScreen if there is some text displayed on the firstScreen. I found an old post (here) where the accepted answer says it is difficult right now and working on a better way ... that post is from 2019 th...

Rodo by Senior
  • 2152 Views
  • 2 replies
  • 1 kudos

Resolved! Re: STM32F769I-DISCO - Really noisy TFT LCD display

Hi everyonei worked fine with MB116-A03 display and now i have the same problem with A09 display. I made the changes available on github:- created the new component nt35510 with the three files (.h .c .html)- and made changes to 4 files: stm32f769i_d...

MikParà by Associate
  • 1970 Views
  • 2 replies
  • 0 kudos

Resolved! TouchGFX and Textarea problem

HelloThis problem has arised when creating a more complex program and I have narrow it down to a single test.project. I have created the usual project for the STM32F769 Disco using TouchGFX 4.20 Designer . I have set only one single TextArea, configu...

jtpgilej by Associate II
  • 3876 Views
  • 4 replies
  • 0 kudos