STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Screen set Visible

Dear all!Normally, Screen  will display in 305ms, the transfer to Screen1. In Main.C, bat_e will be calculated, if bat_e= true, will hide Screen and Screen1 and display Screen 2. can you share me how to do it.

Shaking animation

Hello,I am trying to add warnings to widget when an error happens (shake / judder).I first started looking at the MoveAnimator class but there is no way to "ease" if the startXY == endXY.Other than hand rolling the position myself (as Gaetan shows), ...

Marc_LM by Senior
  • 1109 Views
  • 1 replies
  • 1 kudos

Unable to LTDC ReConfigure/Reinit after LTDC Deinit

  Hi, I am trying to reinitialize the LTDC-TFT LCD controller in a task when I press a button. I am using the STM32H735G-DK kit, which has a TFT LCD. I have created a project using TouchGFX, and it seems the display gets initialized and loaded with...

rakesh1_0-1730545920340.png
rakesh1 by Associate II
  • 3521 Views
  • 7 replies
  • 0 kudos

Resolved! STM32U575ZI + GFX02Z1 - joystick issues

Hi, I'm having a really hard time with the above example TouchGFX Board Setup in TouchGFX Designer 4.24.1.  What should be a really straightforward (supported hardware) project has thus far got me very confused. As a simple test for a slightly more c...

Touchgfx display refresh issues

I am using STM32H757 board which MIPI DSI LCD onboardCreated touchgfx project and disabled RTOS (as I don’t want to use RTOS in my project). Tim6 is used for SYSI am incrementing a value by 1 (variable is declared as global static) on gui from model:...

k_c2024 by Associate II
  • 3610 Views
  • 5 replies
  • 0 kudos