STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Generating LL library for FDCAN

Hi Team,I am working on SIL2/3 compliance project. For this I need to generate and work on LL based libraries instead of HAL libraries.I am using STM32Cube v1.19.0. and working on STM32H753xx and STM32G4A1VET6 series MCU.I am unable to generate LL li...

Abey by Visitor
  • 48 Views
  • 2 replies
  • 0 kudos

STM32F429IGT6 Dual Bank OTA updates

Hi folks,I am trying to implement a dual bank OTA system on my STM32F429IGT6 using DBM1 and BFB2 in the STMCubeProgrammer, but I'm having trouble booting into the second flash region (which I will call app_b from now on, along with app_a for the firs...

STM32 CDC ECM HOST Lib

Hello,I'm working on an adapter USB to Ethernet and it is working only as a DEVICE. Now I would like to do the same but I want my STM to work as HOST.Is ST providing the same code stm32-mw-usb-device but for host?Thanks,G.

Gwen1 by Associate III
  • 103 Views
  • 3 replies
  • 0 kudos

How to test STM32CubeExpansion_STL_G0_V2.0.0

Dear ST,   After signing the NDA agreement, I received STM32CubeExpansion_STL_G0_V2.0.0.   I tried testing the projects for NUCLEO-G071RB in STM32CubeIDE 1.14.1, but to no avail. Edit: Removed screenshots as package is under NDA. After importing the ...

Kolkentu by Associate II
  • 79 Views
  • 4 replies
  • 0 kudos