STM32 MCUs Embedded software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SDRAM + SD-Card intermittent write failure.

I am having issues when writing a buffer that is declared in the external buffer to an SD card. When I tried to download a bulk file (1.5MB), write failure (f_write returns FR_DISK_ERR) would happen at least once during the download process, but if I...

H743 FreeRTOS

HI I m using H743 Nucleo, to write a RTOS program with 2 tasks which gonna access to the same memory location concurrently.. can anyone advise which  RTOS method to use ? Tasks ? Semaphore? Message Queue? 

TCP Socket bare-metal, can it be done?

Hi,I am running a simple TCP server using the lwIP stack and no RTOS. I got help from the "Echo_Server" example offered in most ST eval board packages, everything works fine.I need to accept a single socket connection from the outside and maybe also ...

AndrewST by Associate II
  • 153 Views
  • 11 replies
  • 1 kudos

Resolved! Wrong (duplicated) PWM pulse

I'm a software developer and love electronics, specifically making metal detectors. I'm trying to develop a new Pulse Induction metal detector and I'm using this development board (STM32F407VET6).Although I'm a software developer, I work with high le...

While(1) loop stops executing

Hello,For my project Im checking on a data request by using DMA and UART Idle interrupt. After a few minutes my while loop just stops executing. The code keeps executing the USART1_IRQHandler and doesn't return to the main code anymore. If Im not usi...

mJelmer by Associate
  • 68 Views
  • 3 replies
  • 0 kudos