cancel
Showing results for 
Search instead for 
Did you mean: 

SDRAM + SD-Card intermittent write failure.

cleonb322
Associate III

I am having issues when writing a buffer that is declared in the external buffer to an SD card. When I tried to download a bulk file (1.5MB), write failure (f_write returns FR_DISK_ERR) would happen at least once during the download process, but if I declared the buffer in the internal RAM, I didn't have the problem.   

 

Example of my linker: 

/* Memories definition */

MEMORY

{

RAM (rw) : ORIGIN = 0x20000000, LENGTH = 499K /*512K*/

FLASH (rx) : ORIGIN = 0x8008000, LENGTH = 2048K - 0x8000

SDRAM (rw) : ORIGIN = 0xC0000000, LENGTH = 16M

Memory_B1 (rw) : ORIGIN = 0x2007C000, LENGTH = 0xA0

Memory_B2 (rw) : ORIGIN = 0x2007C0A0, LENGTH = 0xA0

QUADSPI (rw) : ORIGIN = 0x90000000, LENGTH = 16M

}

....

.buff_sec (NOLOAD) :

{

. = ABSOLUTE(0xC0144100);

*(.buff_Section)

} > SDRAM

//code example - buffer definitions

__attribute__((aligned(4))) static FILE_SYS_BUFFER _bulkdwldBuff __attribute__((section(".buff_Section")));

If I remove "__attribute__((section(".buff_Section")))" from the declaration, it works 100% of the time. i tried using "SCB_CleanDCache_by_Addr((uint32_t *)aligned_addr, cache_size);" before f_write but it doesn't help the problem.

I even tried setting up MPU regions for the SDRAM:

MPU_InitStruct.Number = MPU_REGION_NUMBER5;

MPU_InitStruct.BaseAddress = 0xC0000000; // Start of SDRAM

MPU_InitStruct.Size = MPU_REGION_SIZE_16MB; // Adjust to your SDRAM size (ensure correct size)

MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;

MPU_InitStruct.IsCacheable = 0; // Key! Make non-cacheable

MPU_InitStruct.IsBufferable = 0; // Key! Make non-bufferable

MPU_InitStruct.IsShareable = 1; // Optional based on usage

MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;

MPU_InitStruct.SubRegionDisable = 0x00;

MPU_InitStruct.DisableExec = 1; // Disable execution in SDRAM region

HAL_MPU_ConfigRegion(&MPU_InitStruct);

 

 

 

 

5 REPLIES 5
AScha.3
Super User

To check its no problem with cache, just switch off all caches, then test again. (+ MPU not used.)

 

 

If you feel a post has answered your question, please click "Accept as Solution".

The problem seems to be something else and not a cache problem. I have several buffers/structs defined in the external SDRAM, and during the bulk download, I notice that the values in another buffer change/corrupt! SCB_EnableDCache() is commented out, and SCB_CleanDCache_by_Addr() and SCB_InvalidateDCache_by_Addr() are not called.

When writing data to:

static FILE_SYS_BUFFER _bulkdwldBuff __attribute__((section(".buff_Section")));

Sometimes, change values in:

CAN_STRUCT CAN_Struct __attribute__((section(".buff_Section")));

For me just the " Sometimes " sounds suspicious : could be a hardware related problem, so sometimes wrong address on sdram ...? 

Is it custom board ?

+ could you play with sdram timing , just to check, if its timing is a problem ?

If you feel a post has answered your question, please click "Accept as Solution".

I don't think it is an address on sdram because it fails at different points during the downloading of the 1.6MB file. Yes, it is a custom board, and it had some issues with the power supply stability. I was able to fix the power supply issue by using an inductor with a different value. I want to complete as much of the firmware as possible before designing another circuit board. 

I don't think it is a board issue because I am using the same SDRAM for the display frame buffer, and I don't have any issues with it.

ERROR
Senior