STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1802 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4950 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9701 Views
  • 5 replies
  • 3 kudos

Hall Sensor in Steval IPM 30B

I am trying to control BLDC motor with Steval IPM30 B and Nucleo L476RG as controller. In sensor less mode it is working fine but when I am using Hall Sensor it is not rotating at all and its showing speed feedback error at the starting only. How to ...

Screenshot 2024-12-03 122241.png
hu88 by Associate II
  • 3158 Views
  • 7 replies
  • 0 kudos

Resolved! B-G431B-ESC1 motor profiling issue

i have B-G431B-ESC1 board and motor. I can not profile this motor. X-CUBE-MCSDK-6 have issue that when i wrote max speed for example 30 000, my motor is go up to 3 000 which is 10% of max. In order to solve this issue i am using X-CUBE-MCSDK (version...

bcryhun by Associate II
  • 2242 Views
  • 2 replies
  • 0 kudos

EVSPIN32G4 and Quasi-synchronous rectification

Hello, I use the EVSPIN32G4 to test some brushless motors. On ST motor workbench there is an option called: Quasi-synchronous rectification in PWM generation.There is nothing on the board documentation about it. I'am quite familiar with both synchron...

Capture d’écran 2024-12-18 184705.png
DrDhot by Associate
  • 889 Views
  • 0 replies
  • 0 kudos

Resolved! Private schematic review

Hello,Is there a way to get schematic reviewed without sharing it publicly? My company doesn't allow public posts, so wondering if there is any possibility private reviews. Thank you!

How to implement PLL in STM32?

I am trying to implement a Phase Locked Loop in a microcontroller STM32. I have a reference signal and feedback signal which has $\phi$ difference wrt reference signal. For the moment, I am not using a real time feedback signal, rather simulating it ...

zeekzhen by Associate
  • 1189 Views
  • 0 replies
  • 0 kudos

Resolved! ST Motor Control with STLinkV3

Hi all,I have adapted the B-G431B-ESC1 board into a custom design and I am using a STLINK-V3MINIE for programming. I can program the controller and I can communicate via the serial interface.But ST Motor Pilot V1.2.12 does not detect the UART interfa...

Phase loss Motor

HelloI'm trying to figure out how to detect a phase loss on the motor side. I'm looking for a distinction between "loss of one motor phase" and "loss of all motor phases". This can be recognized quite well from the currents measured using the ADC. Ho...

tV1 by Associate
  • 995 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.