STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1726 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4875 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9572 Views
  • 5 replies
  • 3 kudos

Code generation fail in the MC workbench

Hi, I have a project in the MC workbench and I can generate code (for stm32F407) successfully when I use the "Three Shunt Resistors" current reading topology, and the code works well on my board. Now I need to change my board and use the current sens...

post1.jpg post2.jpg post3.jpg post4.jpg
DF_MC by Associate III
  • 1729 Views
  • 5 replies
  • 0 kudos

Resolved! STM32 ZEST Kit & Motor Control Workbench 6.2.1

Dear Sir or Madam,I tried to generate code for the STM32 ZEST Kit consisting of trying to evaluate HSO (while waiting for ZEST approval):1) STEVAL-LVLP012) B-MOTOR-PMSMA13) B-G473E-ZEST1SSince the motor (2) is not available I tried using the Motor Pr...

MoCo by Associate II
  • 10537 Views
  • 11 replies
  • 3 kudos

Resolved! brake function in 6-steps

Hello,I am currently designing an ESC for a small vehicle (around 300g).  I made a first proto board and I use the 6-steps algorithm with an hall sensored motor. I would like to be able to brake. I firstly thought to short all the phases directly to ...

Xavier75 by Associate II
  • 2210 Views
  • 5 replies
  • 0 kudos

EVSPIN32G4 Over Current Protection (OCP)

Hi all , I'm currently using the EVSPIN32G4 evaluation board along with MC Workbench for motor control development, and I'm encountering an issue with Overcurrent Protection (OCP) behavior that I can’t quite resolve.My Setup:Gain Type: External Gain ...

1746582341903.jpg 1746582329251.jpg 1746583672261.jpg
1123 by Associate II
  • 1273 Views
  • 1 replies
  • 0 kudos

Noisy current on STEAVL-PTOOL4A

Hello, I am having a lot of noise of the Id and Iq current. The Eval board is connected to a BLDC, having a hall sensor. I am using the v6.3.2 of the MC Workbench. I am running the Open Loop Current Mode from MC Pilot to make sure that it is the not ...

AnthonyK_0-1747734539732.png
AnthonyK by Associate III
  • 862 Views
  • 1 replies
  • 0 kudos

Resolved! HSO with bus voltage higher than 1000V

Hi,I'm using Motor Control Workbench 6.2.0 with a custom power board that supports a maximum of 1200Vdc. The motor to be controlled also supports a maximum of 1200Vdc.When creating the project, I noticed that on the Power Supply tab, the application ...

RTirapegui_0-1725550937518.png RTirapegui_1-1725551109552.png RTirapegui_2-1725551717399.png

Motor profiler 1.2.9 unable to spin motor

Hi, I am using motor workbench 6.3 along with stm32cube mx 6.12 and stm32cubeIDE 1.16.0. The hardware is a F303RE nucleo board with IHM08M1 motor board. The motor is a generci A2212 1000kV drone motor with a maximum current of 10A. C3, C5, C7 are rem...

IMG_20240821_142029810.jpg code generation.png the measurement is taking too time.png motor profiler setting.png
Sujoy_B by Associate II
  • 2386 Views
  • 3 replies
  • 1 kudos