STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1718 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4870 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9550 Views
  • 5 replies
  • 3 kudos

Resolved! EVSPIN32G06Q1S3 not in CubeMX board selector

I'm trying to program the EVSPIN32G06Q1S3 to run a PMSM, but I attempted to use STM32CubeMX to help with the pinouts and code. The problem is that I can't find the EVSPIN32G06Q1S3 in the board selector. Is there a way to download then import the boar...

Hugo_ by Associate
  • 917 Views
  • 2 replies
  • 0 kudos

Resolved! How can I configure the Motor with low speed

Hi, I'm working on a project in MC Workbench 6.3.2 and trying to configure a motor with a maximum speed of 150 RPM. When I set the "Max. Application Speed" parameter to 150 RPM (as shown in the first picture), I encounter an error related to the "Spe...

maxspeed.jpg sensor_setting.jpg
DF_MC by Associate III
  • 1568 Views
  • 6 replies
  • 2 kudos

MCSDK 6.4.0 Board Designer question

I dump a STEVAL-SPIN3204 board in STMC Board Designer and want to add "Electronic Speed Control" Feature.In Board Designer I had add this feature without error. But in Motor Control WorkBench as attached 1.JPG .We can see ESC feature. But in project ...

Resolved! ADC selection for HSO sensing

Hello STIm trying to generate a HSO compatible FOC board using the STM32G747CEUx but I am not able to select the HSO option for Speed sensing.I've seen the requirement of using atleast two different ADCs for the current sensor and voltage measurement...

Motonaut by Associate
  • 521 Views
  • 2 replies
  • 0 kudos

Does the STEVAL-CTM010V1 support 115200 baudrate ?

Hello,      I use MCWB 6.4.0 & Motor Pilot 6.4.0, STLINK V3 MINIE.      Motor Pilot can not discover STEVAL-CTM010V1 board.      And  I find that MCU can receive datas at buadrate 1200 to 14400, but failed at 19200  or  more fast .      Does the STEV...

wcx8229 by Associate II
  • 731 Views
  • 2 replies
  • 0 kudos

stm32 motor workbench

merhaba topluluk. elimde bir adet f303re kartı ve bir adet ıhm08m1 kartı var.foc kontrol ile bir bldc motor sürmem gerekiyor. ancak bazı sorunlarla karşılaşıyorum.1)nominal deviri 1000rpm girdiğim halde motorpilot arayüzünde 2300rpm e kadar çıkıyor v...

X-NUCLEO-IHM05A1

for this motor controller  X-NUCLEO-IHM05A1. i downloaded zip file from website X-CUBE-SPN5. then after i tried implement with the stm32cubeide. i have a STM32Nucleof401RE microcontroller. I don't understand how to use this file can anyone please gui...

dhva1234 by Associate II
  • 582 Views
  • 2 replies
  • 0 kudos