STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1725 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4873 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9558 Views
  • 5 replies
  • 3 kudos

Resolved! Programmer can't find STEVAL-ESC002V1

Hello,  I am using a STEVAL-ESC002V1 board and I am stuggling to make it work. I want to load the bin file given in STSW-ESC002V1 but the STM32Cube Programmer does not find the board. I am using a STlinkV3Minie connected to the SWD connector.The inst...

ifez by Associate
  • 1501 Views
  • 2 replies
  • 1 kudos

Understanding of Parameters in sto-pll

Hi ST,I am trying to understand sensor less speed measurement using STO-PLL observer I did not get any idea for the parameters F1, F2, gain1 and gain2 parameters from user manual (STM32 motor control SDK user manual) and software code too. could you ...

Rahuld_0-1751360567211.png
Rahuld by Associate III
  • 1191 Views
  • 3 replies
  • 0 kudos

STEVAL-ESC001V1 example code generate failed

1. Hardware / Software setupBoard: STEVAL-ESC001V1 (MCU: STM32F303CBTx)Motor: BullRunning BR2804-1700 kVSTM32 Motor-Control SDK: 5.4.8 (C:\…\MC_SDK_5.4.8)MC Workbench: 5.4.8.21553STM32CubeMX: 5.4.0, 5.6.1, 6.4.0STM32Cube F3 FW: 1.11.3Target tool-chai...

AngHung by Associate
  • 841 Views
  • 3 replies
  • 2 kudos

3V motor control with PWM

Hi everyone, I'm currently working on a project where I'm controlling a small DC motor using a PWM signal, based on the temperature read from an LM35DZ temperature sensor. I'm using an STM32 microcontroller, and generating the PWM signal with Timer2,...

WhatsApp Image 2025-07-01 at 11.23.18.jpeg
Matija1 by Associate II
  • 1532 Views
  • 4 replies
  • 0 kudos

Resolved! power supply on evlservo1 control board

Hello,Is there a way to power the control board of the EVLSERVO1 without using the power board? I would like to just play around with the MCU before connecting to 48V for motor control. The ST-LINK V3SET does not provide any power to the board. Br,Lu...

Lukas47 by Associate II
  • 848 Views
  • 1 replies
  • 1 kudos

Micro controller required for motor control

Hi STM team,I am currently evaluating hardware solutions for a 64 kW BLDC motor control system in a VTOL (Vertical Take-Off and Landing) aerospace application. The project demands high safety assurance and performance, targeting DO-178C DAL-B or high...