STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1820 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4963 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9720 Views
  • 5 replies
  • 3 kudos

Three shunt resistor Current sensing

Hi,While I'm creating custom inverter board for 3 Phase BLDC motor Rail application. I had configured all motor related parameter, while Current sensing section, I have chosen Three Shunt Raw Currents Differential External Gain.I'm getting this error...

VINODC_0-1754994175714.png VINODC_1-1754994370083.png
VINODC by Associate II
  • 750 Views
  • 3 replies
  • 0 kudos

Resolved! EVLSERVO1 unable to connect to stm32CubeProgrammer

Hi,i have a new EVLSERVO1 and a STLINK-V3SET ant try to program my MSDK 6.4.0 generated firmware but i am not able to connect to the bord.  I use the latest STMCubeProgrammer 2 20.0 and the latest stsw-link009 USB Driver.I updated the Firmware on the...

THfl1_0-1754948049667.png THfl1_1-1754948192391.png
THöfl.1 by Associate III
  • 1012 Views
  • 5 replies
  • 0 kudos

"Can't compare values of these types. Allowed comparisons are between two numbers, two strings,..."

2025-08-12 10:04:37,611 调试 [WB_to_MX.lambda$run_gui_mode$0] 参数:[-mx_timeout, -1, -pack, assets/MotorControlPack/MotorControl.zip, -exp, templates/wb-defines_where_and_what.txt, -ftl, templates/wb_ioc_template.ftl, -xdm, E:\STMotorControlWorkbench\640...

EVSPIN32G06Q1S3 and STLINK-V3SET not communicating

I am working with the EVSPIN32G06Q1S3 and the STLINK-V3SET, I have the two programmer/debugger boards mounted on top of each other. Then I have the UART connector connected to the EVSPIN32G06Q1S3 (J5) and the programmer/debugger boards (CN7). I have ...

Hugo_ by Associate
  • 562 Views
  • 2 replies
  • 0 kudos

Resolved! Regular Conversion Manager MCSDK 6.4.0

I have manually migrated from MCSDK 6.2.0 to 6.4.0 for my micro STM32G431RBT6 from the example project as i have seen several changes in the source code and HAL drivers and i want to keep the project upto date for any future changes and can adapt eas...

STuser2_0-1754563002980.png
STuser2 by Senior III
  • 663 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.