STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9547 Views
  • 5 replies
  • 3 kudos

Increasing sensored FOC encoder feedback loop

Hi,   I am trying to create an online angular velocity controller where my torque is dependent on the angular velocity of the motor (motor being driven by the plant). Basically, I want to resist the movement from the plant in a way that keeps the con...

KStew.1 by Associate III
  • 972 Views
  • 1 replies
  • 0 kudos

Resolved! How can I drive the motor with the open loop APIs

Hello Everybody,MCSDK:6.3.2CubeMX: 6.1.4Workbench : 6.3.2 I want to test the motor first with the open loop APIs. I follow the instructions of the user mannual and write the code as follows:My question is: I captured the U, V, and W three-phase wavef...

code1.jpg
DF_MC by Associate III
  • 727 Views
  • 5 replies
  • 0 kudos

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

Trying to use STEVAL-SPIN3204

  Hi I am new to this tools but basically I have tried with 3 different boards STEVAL-SPIN3204  but I am not able to connect the board or do anything useful with it. I have connected the device through USB to my computer, initially LD1 and DL1 where ...

STEVAL-CTM012V1A USART CONNECTION ISSUE

Hi , I am using multiple ST Evaluation Boards and all worked well . However , in one of the board i am facing issue of UART connection . Board is ST   EVAL-CTM012V1A . STMCSDK is 6.3.2, Keil u vision 5 , STM32cube Mx 6.11.1 . Baud rate tried :- 9600...

IC5151_0-1751010555500.png
IC5151 by Associate II
  • 1150 Views
  • 8 replies
  • 1 kudos