User Activity

Hello, I am using a circuit for motor control. comment but sometimes it lights up, I think it's a hardware problem. Can you examine the circuit?  
hi,When I want to generate the code, it says that the STM32CubeMX version is not supported. Even though I downloaded the latest version, it still gives the same problem.  How can I solve this problem?Thank you
hi,When I want to generate the code, it says that the STM32CubeMX version is not supported.Even though I downloaded the latest version, it still gives the same problem.How can I solve this problem?Thank you
Hello,STM32G474RE is the processor model I use.I read ADC from pin PA3 and I read IO from pin PC5. So whether these pins are common pins in the processor hardware? How can I separate these two pins from each other? 
Hello,STM32G474RE is the processor model I use.I read ADC from pin PA3 and I read IO from pin PC5. So whether these pins are common pins in the processor hardware? How can I separate these two pins from each other?
Kudos from
Kudos given to