STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1764 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4916 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9646 Views
  • 5 replies
  • 3 kudos

Facing an error when using MCSDK 6.4.1

Hello,I encountered an error when using MCSDK 6.4.1 (Motor Control Software Development Kit 6.4.1) to configure the STM32G431VBT for using the three-resistor internal operational amplifier and performing external differential gain sampling. I would l...

hang_0-1755912335348.png hang_13-1755913014045.png hang_14-1755913036144.png hang_15-1755913047945.png
一hang by Associate II
  • 1218 Views
  • 5 replies
  • 0 kudos

PWM generation in timer 2

I am using stm32g431c8u6 microcontroller . I have enabled timer 2 channel 3 for alternative pin of PB10 and I have enabled channel 4 for PA3 pin. I set counter perioud 499 and prescaler value =0.When I plug the debugger and run the code only channel ...

Tashenlrana_0-1756361739173.png Tashenlrana_1-1756361772126.png Tashenlrana_2-1756361921155.png

Resolved! Motor pilot application not starting

I have installed MCSDK 6.4.1I can run the workbench (MotorControl Workbench_6.4.1) without any problem.But i cannot run the Motor pilot application.At first there was an error stating "The code execution cannot proceed because MSVCP140.dll was not fo...

B-G431B-ESC1 not able to move the motor

Hi, I am trying to use the disco-B-G431B-ESC1 board to move my gimbal motor. I am using the simpleFOC library example. The problem I am facing is that the motor is not moving. The motor is vibrating at a pole. If I move the motor by force then it vib...

X-NUCLEO-IHM07M1 MC WORKBENCH Fault Problem

 Greetings.I started to study motor control with X-NUCLEO-IHM07M1 as following- MCU : STM32F302R8- PowerBD : X-NUCLEO-IHM07M1- Motor : Bull Running BR2804-1700Kv I just try to make STM32Cube IDE project using MC Workbench 6.4.1 (as described followin...

robotype_0-1755848030553.png robotype_1-1755848197276.png robotype_2-1755848282217.png
robotype by Associate II
  • 1270 Views
  • 7 replies
  • 0 kudos

3 phase BLDCdrivers

i am new to this BLDC motors and i am planning to build a 3-phase motor driver. attached the motor datasheet as well.Can anyone suggest a suitable driver for proof of concept for the attached motor specs.Link: https://www.maxongroup.com/medias/sys_ma...

Resolved! Can I select some other ST MCU in STMC board designer?

Hello Everybody,I'm designing a motor control board using the STM32F405 MCU in an LQFP64 package. When using STMC board designer, I noticed only a limited selection of MCUs is available (please refer to the attached picture ).  Could you advise how t...

bd_design_mcusel.jpg
DF_MC by Associate III
  • 980 Views
  • 3 replies
  • 0 kudos