I am using GBM1008H-150T PMSM motor. Cannot get motor parameters using "Start profile". Motor is noisy and rotates jerkily. I am applying 24V. Specification says the motor has 14 pole pairs and 7 KV.
There is application note AN4457 which introduce UART emulation. And it says all GPIOs can be configures as UART_TX/RX. But how many? Can I use them simultaneously?AN4457 page 6
Hello, I am working with "Mastering The STM32" book and faced with one problem: cannot find the option as in the book to activate any timer using CubeMX. I am using STM32 blue pill STM32F103C8T6. Why I can't find the activate option of timers?
Hello. Why STM32CubeIDE suggesting me to autocomplete u (unsigned type) as a u_int32_t if it doesn't built? However uint32_t works well. What is the difference using u_intXX_t and uintXX_t?
Thanks! I will continue learning and will read the general purpose timers chapter. Seems like I asked that question too early since there is not any basic timer