STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1744 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4892 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9595 Views
  • 5 replies
  • 3 kudos

Current surge with hall sensor at engine start

Hello Everybody,MCSDK : 6.3.2CubeMX: 6.3.2Workbench : 6.3.2Cube IDE : 1.18.1Hardware : Custom but based on EVLDRIVE101-HPDMotor : PMSM 28V - 2 pole pairs - Rmp = 14K - rated current = 13A - Primary sensor : Hall, Secondary sensor Observer+PLL (sensor...

Oli49 by Associate II
  • 1077 Views
  • 5 replies
  • 0 kudos

Clarification on the Hall Interrupt

I always observe a spike when i start to run the motor which leads to audible noise or jerk when i went through the code to modify i have observed the variable hAux little confusing request to please confirm if it is intended __weak void *HALL_TIMx_C...

STuser2_0-1757419669568.png STuser2_1-1757419688398.png
STuser2 by Senior III
  • 1258 Views
  • 6 replies
  • 0 kudos