STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1743 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4892 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9594 Views
  • 5 replies
  • 3 kudos

B-G431B-ESC1: Encoder-Based Speed Control Failure

System Details:MCSDK Version: 6.4Tool: MC Workbench 6.4.0Control Board: B-G431B-ESC1Motor: GL40 KV210Encoder: AS5047P with quadrature outputHello,I'm new to BLDC and FOC motor control and am currently trying to implement speed control using a quadrat...

Screenshot 2025-08-12 at 16.17.48.png Screenshot 2025-08-12 at 17.06.15.png
RobO1 by Associate
  • 891 Views
  • 1 replies
  • 0 kudos

A hardware fault is reported after pressing a button to initiate the pre-charge process (6.4.0 SDK/STM32G431)

您好,我已经在STM32G431上成功配置了 6.4.0 SDK 包。 但是,当我按下按钮并开始预充电过程时,报告了硬件故障。 如果我在预充电过程中将上侧 PWM 波的刻度值从 0% 更改为 90%,程序将在 RUN 后进入 STOP 状态,然后进入故障状态。故障代码为 40,定义为 #define MC_BREAK_IN ((uint16_t)0x0040) /**< @brief 错误:紧急输入(过流)。 */ Post edited by ST moderator to follow th...

BY1 by Associate II
  • 1097 Views
  • 8 replies
  • 0 kudos

Motor Control Issue with MCSDK 6.4.0

Hello,I am working with the STM32F303E-EVAL control board and the STEVAL-IPMNM2S power board, using IAR Embedded Workbench 9.40.I have struggled to get the motor running. I initially tried both MCSDK versions 9.3.2 and 9.4.0 separately, but in most c...

Resolved! Motor pilot firmware for EVLSERVO1 board

Hello,I had the motor profiling experience to get motor mechanical and electrical parameters using EVSPIN32G4 boardsas following:Now I'm trying to start the project for controlling a new high power motor with EVLSERVO1 board. But, I couldn't find the...

rokkie68_1-1757497951533.png rokkie68_0-1757497369140.png
rokkie68 by Associate
  • 883 Views
  • 1 replies
  • 0 kudos

Resolved! Motor forward/reverse transition issue in ST Motor Pilot

Hi all,I’m currently using the EVSPIN32G4 development board for a drone project. I’m controlling motor forward and reverse using ST Motor Pilot.I’ve noticed that when switching from forward to reverse, there’s a short pause before the motor starts sp...

1123 by Associate II
  • 940 Views
  • 1 replies
  • 0 kudos