STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1758 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4909 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9629 Views
  • 5 replies
  • 3 kudos

Position Extraction from Hall sensors

Dear All,I am currently working on a 10 kW motor drive for controlling a PMSM in an automotive traction application, utilizing a Field-Oriented Control (FOC) algorithm. I am facing a challenge with position extraction from the motor’s Hall sensors.Th...

engeek by Associate
  • 759 Views
  • 1 replies
  • 0 kudos

STSPIN233 current sensing amplification

Hi there;I'm trying to muddle my way through my first design with a motor driver that includes current sensing. This is for a battery-powered device, operating with an stm32f4 at 3.3v. My motor is a small gimbal-style motor, which I intend to run at ...

sb_st by Senior II
  • 1733 Views
  • 7 replies
  • 0 kudos

Resolved! STSPIN32G4 – Unable to Drive MOSFETs

Hello everyone,I’m working on a project using the STSPIN32G4 and running into an issue where the MOSFETs are not switching as expected. I’d really appreciate some guidance from the community.Setup:MCU: STSPIN32G4 (integrated STM32G4 + gate driver)Pow...

suyog1_0-1756129949590.png suyog1_1-1756129984502.png
suyog1 by Associate II
  • 1838 Views
  • 3 replies
  • 0 kudos