STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1610 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4759 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9486 Views
  • 5 replies
  • 3 kudos

Problem with my BEMF (ESC control motor)

Hello ! I'm making a ESC for my BLDC motor. I used a STM32 (to generate my PWM), 3 IR2101 mosfet drivers (https://www.infineon.com/dgdl/ir2101.pdf?fileId=5546d462533600a4015355c7a755166c) and 6 mosfets to control the differents phases of the motor.He...

0693W000005AWlJQAW.jpg 0693W000005AWlOQAW.png 0693W000005AWlYQAW.jpg 0693W000005AWlsQAG.jpg
ET_FR by Associate
  • 1664 Views
  • 1 replies
  • 0 kudos

How to update 2018 STM32F3 Motor Control Hands-On Workshop to use current versions of software on Windows 10 and port to macOS Big Sur?

Folks, I was pleased to attend this workshop in Santa Clara, CA, two years ago and receive the hardware (Nucleo-F302R8, X-Nucleo-IHM07M1, small BLDC motor and power adapter) and workshop software (bundled in an installer). Still have all of this, in...

Resolved! STEVAL-SPIN3201 SWD Programming

STEVAL-SPIN3201After looking at the schematic i can see that there is a second MCU to 'control' the STSPIN32F0. This second MCU has a STLINK connector for programming. My question is ; Is it possible to program the STSPIN32F0 directly and not have to...

PKAci.1 by Associate II
  • 1671 Views
  • 2 replies
  • 0 kudos

Resolved! problem with SPI daisy chain

Hello,I am using IHM02A1 expansion board (on top of L073RZ), which has two L6470 connected in a daisy chain configuration. I cannot receive any data from the devices. What do you think the reason can be ?Below is the bus status of a reset and get par...

0693W000006FZgkQAG.png
mete by Senior II
  • 3944 Views
  • 6 replies
  • 0 kudos

B-G431B-ESC1 has issues powering a BLDC pump application

I have a BLDC fuel lift pump that I would like to power using the B-G431B-ESC1 board.I have gone through the issues as described with the Y version of the µC, and can test the system using the motor profiler.This program is able to spin up my device ...

GStou by Associate II
  • 1041 Views
  • 1 replies
  • 0 kudos