STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1740 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4888 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9587 Views
  • 5 replies
  • 3 kudos

STM32H7 motor control support?

Anyone know when/if the H7 series will have more motor control support? The F series can't do what I need and only 1 chip (which has an eval board) can be used in MCWB but it is extremely limited.

GBuke.1 by Associate
  • 3469 Views
  • 6 replies
  • 1 kudos

Resolved! NEW X-CUBE-MCSDK version 5.4.5 available

Dear Motor Control customers and #[STM32 Motor Control]​ community members,We are very glad to announce the new X-Cube Motor Control SDK 5.4.5.This version is fully compatible with new CubeMX 6.1 and is still available at: https://www.st.com/en/embed...

Why is the MCSDK not using floating point algorithms?

Since I'm still fairly new to the STM / Arm world, I wonder why, for example, the X-CUBE MCSDK does NOT use the floating point algorithm for devices that have a hardware floating point unit. Are there special things to watch out for when using floati...

ben5en by Associate II
  • 1314 Views
  • 2 replies
  • 1 kudos

Why does VBUS voltage always show 0V (Under Voltage Fault) in Monitor section of ST Motor Control workbench?

I have developed a custom board using STSPIN32F0A for bldc motor control application. When I am trying to test with Bull Running BR2804 motor, after configuration of pins when I check in Monitor Section, VBUS voltage is 0 Volt and a continuous Underv...

how does the divider work in PID tuning?

I am using NUCLEO-F303RE, X-NUCLEO-IHM08M1, MotorControl Workbench 5.4.4 and STM32CubeMX 5.5.0. I have managed to generate a project as position control and it seems to work fine however I am wondering if I can improve further the performance of the ...

msingh by Senior
  • 1513 Views
  • 2 replies
  • 1 kudos

Resolved! evspin32f0601s1 (6-step control in workbench)

I bought the evspin32f0601s1 board.In the data sheet"Sensored or sensorless 6-step algorithm"It is described like this...Is it not possible to select 6-step in the st motor control workbench?And since there is no detailed information about the workbe...

DLee.10 by Associate
  • 1171 Views
  • 1 replies
  • 1 kudos

Resolved! [CRITICAL HW BUG + FIX] STEVAL SPIN3204 board: maximum motor current not reaching 16A as claimed

PCB layout of STEVAL STSPIN3204 board contais critical bug as explained in attached report which prevents the design to work up to claimed 16Arms. This bug creates extreme radiated emissions (affecting nearby instruments) and prevents the proper func...