STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1735 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4881 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9580 Views
  • 5 replies
  • 3 kudos

FOC SDK + HALL not on TIMx

Posted on January 06, 2016 at 19:54Hello, I've just designed and populated some prototyping boards which happen to connect the HALL sensor not on the correct TIM2-5 CHX pins. Instead of just throwing all in the garbage, I was wondering if is there a...

vmatos by Associate II
  • 2290 Views
  • 6 replies
  • 0 kudos

STM32 FOC SDK with another compiler

Posted on January 18, 2016 at 15:34I am wondering if I can use STM32 FOC SDK with a compiler other than IAR EWARM or Keil MDK-ARM. I have looked up to a document (presentation slide) named ''STM32 PMSM FOC SDK 4.2 - Hands on workshop with hardware ...

FOC Open Loop reverse

Posted on January 28, 2016 at 19:23Hello, I'm currently using Open loop mode for debugging my hardware, current readings and such. I have found by trial and error the best values for the offset and slope of the V/f curve, such that the motors work o...

vmatos by Associate II
  • 1086 Views
  • 2 replies
  • 0 kudos

STEVAL-IHM040V1 with FOC SDK

Posted on February 26, 2016 at 14:33I have obtained a STEVAL-IHM040v1 board a while ago and worked on it with six-step motor commutation method. But now, İ have to use it with FOC method, so I am trying to use STM32 PMSM FOC SDK in order to configur...

STM32 FOC SDK & CubeMX

Posted on March 15, 2016 at 15:44hi! Can be STM32 FOC SDK & CubeMX generated code used in same project? We already have some libraries based on CubeMX. 

vromanov by Associate II
  • 1486 Views
  • 2 replies
  • 0 kudos

Problem to build example with iar 7.4

Posted on March 24, 2016 at 18:42Hi, i have some problems to build a project for P-Nucleo IHM001_singledrive kit !When i open the project it said me that some options are broken and when i build the project (after use workbench tool to configure the...

idealsim by Associate II
  • 1902 Views
  • 3 replies
  • 0 kudos

Issue with FOC sdk 4.2 and stm3210B eval kit

Posted on March 25, 2016 at 16:04Hi i'm trying to work with our STM3210B eval kit (shinano MB459) but i have some problem to use it. When i launch ST Motor Control Workbench : - Choose example project STM3210B-Eval-MB459-Shinano - Check the values o...

idealsim by Associate II
  • 1317 Views
  • 2 replies
  • 0 kudos

Problems with ICS and Hall Sensors on FOC SDK 4.1

Posted on March 29, 2016 at 11:00Hi, we are using FOC SDK 4.1 with ICS current sensing and State Observer + PLL. A Motor with 21 pole pairs and Rs 11mOhms and Ls 0,017mH runs up to 6000 rpm very well.  Now changing to Speed / Feedback with Hall Sens...