cancel
Showing results for 
Search instead for 
Did you mean: 

high side and low side pwm idle state

Low Yik Seong
Associate III
Posted on April 29, 2018 at 16:41

Hi, I would like to ask what is the function of pwm idle state which can be selected in drive management in sdk 5.0? It only can be turn off as I tried turn them on they would be fatal error as I compile the code.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards