STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1720 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4871 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9555 Views
  • 5 replies
  • 3 kudos

What is the Hall sensor MTPA?

What is MTPA in the MC workbench speed position feedback management --> Hall sensors? This is NOT the Maximum Torque Per Amp, I believe. Any reference for this?Thanks for reading.

0693W000002liptQAA.png
hmc by Associate III
  • 2224 Views
  • 2 replies
  • 0 kudos

current limit for b-g431b-esc1

Hello,i'm using a b-g431b-esc1 with a 12 V sm-pmsm motor. After running the motor profiler and the motor control workbench, i've played with the cube ide. I have noticed the motor doesn't draw more than 1,6 A, but max current was set to ~5 A in the m...

cz by Associate
  • 1337 Views
  • 2 replies
  • 0 kudos

Resolved! Is this a 120 or 60 deg displacement angle hall motor?

Hello forum! I am trying to characterize a motor for experimentation with the workbench. I spun the rotor with a hand drill and got the following waveform, with the first 3 channels being H1, H2, H3 and the analog voltage being the back-EMF from th...

0693W000003QjGhQAK.png 0693W000003QjGrQAK.jpg
hmc by Associate III
  • 8774 Views
  • 8 replies
  • 1 kudos

Resolved! BLDC motor: How to archive higher startup torque?

Hi ST CommunityI am working on a project where I want to use a BLDC motor for a screwdriving process. The setup is based on the B-G431B-ESC1 and a Maxon motor https://www.maxongroup.com/maxon/view/product/651618 (with a 6:1 gear added). The motor con...

JA.1 by Associate III
  • 4930 Views
  • 5 replies
  • 0 kudos

Resolved! Is there a way to fine-tune motor parameters (final ramp value, speed ramp up...) in the motor workbench without systematically re-generating code from Motor Control Workbench

Hi !Is there a way to fine-tune motor parameters (final ramp value, speed ramp up...) in the motor workbench without systematically re-generting code from Motor Control Workbench and then Cube-MX everytime every time I'd like to adjust a parameter ?I...

Luczia by Associate II
  • 2162 Views
  • 4 replies
  • 0 kudos