STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1719 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4870 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9555 Views
  • 5 replies
  • 3 kudos

I like to know why can not read the motor parameters from my evaluation board STEVAL-SPIN3202 using the ST Motor Profiler software and i need to buy an new board B-G431B-ESC1?

My company develop a new BLDC Drive board in order to control a BLDC Motor For use in automatic doors mechanism.i attach the datasheet of the motor. The electrical parameters of motor is the following:1. Number of polar pairs : 22.Max.application spe...

SVlac.1 by Associate
  • 1908 Views
  • 2 replies
  • 0 kudos

Resolved! The protocol of Motor control example.

When we're using Motor Control Workbench to control the motor, we can get the motor information and control the motor through Motor Control Workbench. Is this information available via UART?We need to know how Motor Control Workbench communicates wit...

Resolved! STEVAL-ESC001V1 - Workbench example doesn't work

Hi! I am trying to control sensorless BLDC motor using STEVAL-ESC001V1.I finished profiling my motor and working on the example on Workbench(STEVAL-ESC001V1 electronic speed control 5.4.0).I opened the example on the workbench and set the motor param...

Slee.3 by Associate II
  • 2195 Views
  • 5 replies
  • 0 kudos

Resolved! Output phase current being limited to 200A

Hi folksWe have a 3-shunt sensor-less FOC solution for running a PMSM motor generated from STM32 Motor Control Workbench (ver 5.4.4). The max readable current is upwards of 500A. However, we find that the phase current gets limited to 200A peak. When...

PAlva.1 by Associate
  • 2579 Views
  • 4 replies
  • 0 kudos

How to implement speed feedback with B-G431B-ESC1 . I am trying to use this ESC to drive a hoverboard hub motor. Motor profiler works, and I can build an application that lets me run at max speed. Need speed feedb

I am trying to use this ESC to drive a hoverboard hub motor. Motor profiler works, and I can build an application that lets me run at max speed. Need speed feedback to control torque at lower speeds. The motor has both hall sensors and an encoder in...

MCohn.1 by Associate
  • 1324 Views
  • 2 replies
  • 0 kudos

Resolved! Hall Sensor Control w/ STEVAL-SPIN3202

I am using the MC Workbench tool to drive a 3-Phase BLDC Motor with Hall Sensors. I have enabled the hall sensors in the workbench, downloaded the code and flashed my board. How do I actually use the Hall sensor to control the speed? No matter what s...

nmamore by Associate II
  • 3347 Views
  • 6 replies
  • 0 kudos