STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1735 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4882 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9582 Views
  • 5 replies
  • 3 kudos

X-NUCLEO-IHM08M1 peak current higher than 30A ?

What would be the maximum safe peak current for the IHM08M1 board ( 0.5 sec)?I know that the board has a hardware over-current protection kicking in at 30 A. But the STL220N6F7 FETs are rated higher.Also, while configuring the combo X-NUCLEO-IHM08M1 ...

Jay1 by Associate II
  • 1034 Views
  • 1 replies
  • 0 kudos

Motor stops during ramp-up

I could use some help in getting my motor controller through starting the motor. It tries, but always fails to completely start up.I'm working on developing a custom motor control demonstrator board, built with discrete components in the power stage....

0690X000008A7kBQAS.png 0690X000008A7kkQAC.png 0690X000008A7lOQAS.png 0690X000008A7n6QAC.png
RKeny by Associate II
  • 1980 Views
  • 4 replies
  • 0 kudos

When executing the Project Generation command from ST Motor Control Workbench I always get a javax.net.ssl.SSLHandshakeException error showing.

Version info:  MC Workbench      : 5.3.2.18569 WB_to_Mx          : 0.15.6.template-19-01-16 STM32CubeMX       : 5.1.0 MC Firmware Library: 5.3.3Generation options:  Target Toolchain  : ST TrueSTUDIO Target Driver     : HAL - Hardware Abstraction Laye...

Steval Spin3202 - Motor doesn't work ("over-current") ?

Hello,i want to test a BLDC-Motor with the STEVAL-SPIN3202 board. I followed the steps of the datasheet "Using STM32 motor control workbench with STSPIN32F0" to configure the library and generate the code. If i want to start the Motor, I directly get...

TKlei.5 by Associate III
  • 1333 Views
  • 4 replies
  • 1 kudos

MCSDK 5.3.3: code wont execute_ TIM1

Hi,I'm developing an Motor application using F446RE and MCSKD on custom board and custom motor control project, but the program never reaches the user code while loop. I generated the code with ST Motor Control Worbench with 5.2.0 Cube MX andFirmwar...

GBeno by Associate
  • 943 Views
  • 1 replies
  • 0 kudos

I am getting this warring message "These IPs still have some not configured or wrong parameter values:[ADC1]" when trying to generate code on ST Motor Control Workbench

HI,I'm trying to use ST Motor Control Workbench to make a project for control PMSM Motor,But when i click on generate code.I get this warring message "These IPs still have some not configured or wrong parameter values:[ADC1] Do you still want to gen...

Mr.SU by Associate II
  • 1847 Views
  • 5 replies
  • 0 kudos

Steval-spin3201 hall sensors connection.

Hello!I'm trying to work with steval-spin3201 board, i have AMETEC minijammer bldc motor with three hall sensors on board, ST Motor Control Workbench with Atolic True studio. First i tried sensor-less control and it's works fine with some tuning. But...

Roman by Associate II
  • 1689 Views
  • 3 replies
  • 0 kudos

MCSDK-5.4.0 to CubeIDE problem

Using "Motor Control Workbench" I created a project for the following hardware:NUCLEO-F303RE + X-NUCLEO-IHM16M1.I did not make any changes to the standard configuration.I generated the files by setting the TARGET to CubeIDE with firmware package FW V...

MCSKD 5.4.0 HardFault

I did some tests using the MCSDK 5.4.0, I generated the project using MC WorkBench for TrueStudio and CubeMX 5.2.1.The hardware consists of NUCLEO-F303RE and X-NUCLEO-IHM16M1.The problem is the following: when I try to start the engine with WorkBench...

0690X000008ichgQAA.jpg 0690X000008iciFQAQ.jpg 0690X000008icioQAA.jpg