2019-04-29 8:23 AM
Hi,
I'm developing an Motor application using F446RE and MCSKD on custom board and custom motor control project, but the program never reaches the user code while loop.
I generated the code with ST Motor Control Worbench with 5.2.0 Cube MX andFirmware package version V1.24.1. And Build that with TrueStudio.
I commented these lines so that the code turns and can communicate in uart with ST workbench:
HAL_NVIC_SetPriority(TIM1_BRK_TIM9_IRQn, 4, 1);
HAL_NVIC_EnableIRQ(TIM1_BRK_TIM9_IRQn);
I could test the rest of the code: it works. ADC reads the value of vbus
Do you have an idea to use the TIMER 1 ?
Thanks you !
2021-06-22 1:36 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards