STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1735 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4881 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9580 Views
  • 5 replies
  • 3 kudos

Using STM32F103VC in MC workbench

Hi, I have some question on mcu selection in MC workbench. As I have previous build an application based on STM32F103VC, I would like to use MC workbench to do configration. However, i cannot select it from the list. Are there any other solution? Tha...

Ysiu by Associate II
  • 1144 Views
  • 2 replies
  • 0 kudos

Drive 48V Conveyor Drum Motor using STEVAL-SPIN3201

Hello Community,I have purchased a STEVAL-SPIN3201 eval board last week. I want to drive a 48V Drum motor using this eval board with Motor Control Workbench 5.40. But I don't have the full motor parameters. Based on the user manual UM2152, the motor...

0690X000009YKdRQAW.jpg
LXian.0 by Associate II
  • 1872 Views
  • 3 replies
  • 0 kudos

Motor control Workbench is generating code with errors

i am using STEVAL-SPIN3201 development board for the project.first i start the workbench and give the board details then after setting i give to generate code.the workbench is giving the code with errors.why this happens...?i am attaching my log whic...

NK.13 by Associate II
  • 920 Views
  • 3 replies
  • 0 kudos

Cannot connect with stm32f303VC in monitor

After I load the program into the MCU, I tried to connect the device in the monitor and it show the message "connection failed! No response. check the communication cable, the power on the board or the baudrate". I have checked the baud rate and port...

0690X000009Ys2EQAS.png
Ysiu by Associate II
  • 1150 Views
  • 2 replies
  • 0 kudos

Error in code which is generated by St motor workbench

i have generated code from motor control workbench and when i build this code the error came as,region `FLASH' overflowed by 18000 bytes StSpin_Hall_24_07 C/C++ ProblemStSpin_Hall_24_07.elf section `.text' will not fit in region `FLASH' StSpin_Hall_2...

NK.13 by Associate II
  • 939 Views
  • 1 replies
  • 0 kudos

Does STM32F303RE support dual motor drive?

Hi there, I am using ststem workbench for stm32, cube mx v 5.3 and mcsdk 5.4. I want to develop a dual motor application with stm32f303re. However, after I generate the code and upload it. It cannot connect through the monitor. (Works for single mot...

Ysiu by Associate II
  • 1429 Views
  • 2 replies
  • 0 kudos