cancel
Showing results for 
Search instead for 
Did you mean: 

Steval Spin3202 - Motor doesn't work ("over-current") ?

TKlei.5
Associate III

Hello,

i want to test a BLDC-Motor with the STEVAL-SPIN3202 board. I followed the steps of the datasheet "Using STM32 motor control workbench with STSPIN32F0" to configure the library and generate the code.

If i want to start the Motor, I directly get the fault "over-current" and the Motor doesn't roate?

Can anybody help me?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
TKlei.5
Associate III

UPDATE: If i start the motor now, the board disconnect immediately and the motor whine. Sometimes the motor move a little bit.

CSzat
Associate II

Good luck...

Same issue here...

I also had the board "disconnect" from the Motor Control Workbench when it "faulted".

This should never be the case from a startup failure.

This software/hardware is very "flaky".

Sometimes, even when the STEVAL-SPIN3202 does successfully connect to the Motor Control Workbench, it does not show it as "Connected".

TKlei.5
Associate III

I tried a BLDC-motor with hall-sensors and without hall-sensors and also a small and a bigger motor. I always get the same result.

Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards