STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9547 Views
  • 5 replies
  • 3 kudos

FOC Motor Direction Control

I've implemented an FOC motor control algorithm from scratch (e.g. not using any libraries) and it works well. I'm generating sine waves to drive the MOSFETs via a lookup table.All this works and the motor turns in an anti-clockwise direction. How do...

jerry2 by Senior
  • 1694 Views
  • 1 replies
  • 1 kudos

How to control stepper motor using STM32MP157?

Hello, I want to to know how to control the Acceleration and deceleration of stepping motor using stm32mp157, I think It needs config the TIM2(for example) to one pulse mode and update the new period and enable when interrupt occurs (MOTOR_PUL_IRQHa...

Hi! I can't make the engine spin! I am using NUCLEO-F446RE and X-NUCLEO-IHM08M1. Engine PL57BLF01.

Hi!How to make a project with a motor in the "speed control" mode without using Hall sensors, but using an incremental encoder. With a simple replacement in the "MotorControl Workbench", the properties of the motor and the properties of the speed sen...

X-NUCLEO-IHM07M1 Current Sensing

Anyone know the transfer function of the current sense path (shunt resisters->opamp->ADC) on the X-NUCLEO-IHM07M1? It's not worked out in the user manual and if someone has it it would save me some time.Thanks!

jerry2 by Senior
  • 787 Views
  • 0 replies
  • 0 kudos

Any suggestions on increasing motor speed resolution?

I am operating a low inertia BLDC Motor with the STM32 FOC Motor control library. I have modified the code to add an outermost loop that provides phase lock control to an external reference.The one limitation I have is that I think the inner speed l...

BTrem.1 by Senior II
  • 2814 Views
  • 4 replies
  • 0 kudos