cancel
Showing results for 
Search instead for 
Did you mean: 

Stimulate error on motor

JRoja.16
Associate

I use Lib version 4.3 to control SM-PMSM.

The motor can run smoothly.

However I would like to simulate 2 error hereafter.

  • SW error (FOC Frequncy cannot be sustainable)
  • Start up fail.

I would like to check these 2 error without modify code.

PS.I have locked rotor when start ,it shows under-power error instead of Start up fail.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards