cancel
Showing results for 
Search instead for 
Did you mean: 

HFI with STEVAL-IHM042V1

jvankuilenburg
Associate II
Posted on March 25, 2015 at 13:38

Hi,

I like to test the HFI function on the STEVAL-IHM042V1. Without HFI is the motor running well. But how can I implemented the HFI? I followed the instruction of UM1052 page 65. But I can not configure the DAC in the STMCWB. Because DAC1 is used for the OCP and DAC2-pin is input for the MC1currentA. What's the best way to do this?

Thanks,
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards