User Activity

Posted on May 11, 2012 at 15:45Hello, has anyone tried out to implement a sinusoidal commutation for STM32 controllers? I'm already working with a block commutation quite similar to that: http://www.mikrocontroller.net/articles/STM32_BLDC_Control_wi...
Posted on April 11, 2012 at 16:34Hello, I'm a bit confused about the timer usage for the Hall sensors on the STM3210B-EVAL board. The encoder signals (which are used for the hall signals too) are placed on the GPIOs PA0, PA1 and PA2 and timer TIM2 i...
Posted on March 07, 2012 at 14:35Hi, we have problems in using the STEVAL-IHM031V1 power stage. As this is a quite fuzzy problem, we hope someone has some hints for us. Our test setup is a STM3210E-EVAL Board, the named power stage and an approp. ...
Posted on February 15, 2012 at 16:19Hello, I want to use a a advanced control timer (TIM8) of my STM32F103ZG (on STM3210E-EVAL) for motor control. I have problems generating the PWM signal at the right time. I initialize the timer the same way as in...
Posted on February 08, 2012 at 15:30Hallo, is it possible to drive two motors with this eval board? I don't want to drive them simultaneously and independently but ''mutual exclusive'', i.e. I have one enable signal for every motor, while only one ...