STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4870 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9549 Views
  • 5 replies
  • 3 kudos

MCSDK 5.Y.4 6 step sensorless control compiler errors

Hi, I am using STEVAL-SPIN32F04 dev kit to start my learning curve on STMC. I opened a example project of MC Workbench 5.Y.4 " and simply modify the speed sensor algorithm to observer+PLL and then I got compiling errors : Error[Pe020]: identifier "st...

YWang.15 by Associate II
  • 1267 Views
  • 1 replies
  • 0 kudos

Hall electrical phase shift?

Hello Friends.May you help me?In Section 8.3 (hall sensor feedback processing) of STM32F SOC SDK manual. This section mentions to Hall electrical phase shift.So, could you tell me how to get the Hall electrical phase shift? what kind of equipment can...

Vnguy.1 by Associate II
  • 2114 Views
  • 3 replies
  • 0 kudos

Start-up issues with DN4240S24 motor, Motor Pilot shows it goes into RUN state but then begins to vibrate and does not spin.

I am working with a DN4240S24 motor, to do some tests using the motor control SDK, but I am having trouble with the start-up. This is my first time dealing with motor control, so I apologize in advance if I don't grasp certain concepts right away.The...

0693W00000FD8CkQAL.png 0693W00000FD8G8QAL.png 0693W00000FD8RaQAL.jpg 0693W00000FD8Q3QAL.png
GLamb.1 by Associate
  • 2363 Views
  • 3 replies
  • 0 kudos

Resolved! How can I adjust hidden parameters in STM32CubeMX

Opening the example ACIM-STM32G431 .ioc file in a text editor (notepad) shows hundreds of hidden options:I am trying to imitate it through CubeMX, but the parameter settings are not listed under MotorControl. I have matched all the other parameters. ...

0693W00000QKaIZQA1.png
Dane._.T by Associate II
  • 1296 Views
  • 1 replies
  • 1 kudos

Using 2 shunts only

I designed my own motor controller board and it works fine. For the next revision, I am looking into reducing parts count and simplifying schematics a bit. In the sense control area, I have tested the option of using the internal gain for the OpAmps ...

PCama.1 by Associate III
  • 2607 Views
  • 4 replies
  • 0 kudos