STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9547 Views
  • 5 replies
  • 3 kudos

Resolved! F401RE + IHM16M1

HelloI am using the combination of F401RE and IHM16M1 for a project in my lab to drive a 24V BLDC Motor (max RPM 5000). Issues:1) I am unable to select the above combination in the Motor Profiler.2) When I try to generate code using Motor Control Wor...

0693W00000QNbhCQAT.png
AChha.1 by Associate II
  • 7726 Views
  • 14 replies
  • 0 kudos

Resolved! MC SDK not work with MCU Stop mode

Dears,Currently I'm working on a BLDC project, and with the MC SDK, we can control the motor.And we also want to make the MCU(STM32F4) into STOP mode to save some power, the issue is the MCU can not goes into STOP mode, anyone tried this before?​The ...

0693W00000Sv4dmQAB.jpg 0693W00000Sv4dwQAB.jpg
Guopeng by Associate II
  • 9914 Views
  • 10 replies
  • 1 kudos

Tips for X-NUCLEO-IHM03A1 with NUCLEO-G431RB

I've got an X-NUCLEO-IHM03A1 (the PowerSTEP based board) and a NUCLEO-G431RB. I'd like to start on the software to get them working together. However, I'm new to STM32 development. I'm not sure of how I should proceed. Would it be easier to start wit...

ECC01 by Associate
  • 845 Views
  • 0 replies
  • 0 kudos

How to get started with STEVAL-SPIN3202

I only want to have the motor to spin as a kitten but ..Hereby I share you my road to hell and frustrations .Tried to get it working with the example and MCSDK_5.Y.4saved it on an empty location and no renameChange nothing for the moment and pusg...

0693W00000QLEH6QAP.png 0693W00000QLEJ8QAP.png 0693W00000QLEJwQAP.png 0693W00000QLEXZQA5.png
JDedu.1 by Associate II
  • 1513 Views
  • 3 replies
  • 0 kudos

PQD_CalcElMotorPower

We are using STM32F301 micro along with 5.4.4 motor control SDK. We found that at different speeds we get different power measurments for the same amount of power output of the motor.Is this due to the fact that PQD_CalcElMotorPower() does not use po...

COkta.1 by Associate
  • 1197 Views
  • 0 replies
  • 0 kudos