STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9547 Views
  • 5 replies
  • 3 kudos

[Bug Report MCSDK 6.0.0] Overvoltage and overcurrent flags inverted when overvoltage protection is disabled

Hello,Actual behavior:While I have deactivated the overvoltage protection in Motor Control Workbench, I still get the overvoltage fault flags that is sometimes set (when my motors brakes abruptly).My setup: 4-poles BLDC motor, MCSDK 6.0.0, Nucleo G47...

0693W00000SwMPfQAN.png

Resolved! STEVAL-SPIN3202. Got it turning. Now need a guidance on where / what file and how I can control the speed.

Hi All,Got it turning. Now need a guidance on where / what file and how I can control the speed. SDK 5.4.8.6S_STEVAL3202_SL_VM example.Monitor connects well.I can start the motor.Final ramp speed does not work. The only use - setting the direction of...

EShaw.1 by Associate II
  • 8532 Views
  • 19 replies
  • 0 kudos

Is it possible to remove PID from BLDC 6 step SDK

Hello, I am working on a project that requires control the motor speed by adjusting bus voltage. The PWM width shall be consistent. The motor bus voltage is controlled by another ST micro. Is this a possible approach? What documents/ examples I can r...

YWang.15 by Associate II
  • 775 Views
  • 0 replies
  • 1 kudos