Skip to main content
CHuan.8
Associate
October 13, 2021
Question

On the fly change between speed and torque control mode?

My question is how to on the fly change between speed and torque control mode.

Is there any tips or example codes available?

Thx!

​

This topic has been closed for replies.

1 reply

CKlei.1
Associate II
November 17, 2021

Hey CHuan

I did some tests with changing the mode on the fly. In my application, I use torque mode for run up and switch to speed mode when reached a certain speed. I get it running but not as smooth as I would like.

To change from torque mode to seed mode, I monitor the actual speed of the motor. When reaching a certain limit, I programm a speed ramp with the actual Speed and zero rampup time.

In the next loop, I control if this command was executed. If so, I then programm a new ramp with the speed setPoint & desired ramp time.

If you have found a better solution in the meantime, I'll be interested in it.

Regards

Chris