Skip to main content
VD.3
Associate
November 15, 2021
Solved

Help on regenerative Braking for electric vehicles.

  • November 15, 2021
  • 2 replies
  • 1929 views

I am really struggling hard to understand the regenerative braking for electric vehicles for 48V systems. My main doubt is if the motor back emf is less than battery voltage, how does it do generation. The motor is PMSM with sinusoidal back emf and i am trying to control using FOC. Please advise. Basic explanation and any websites or articles will really help.

This topic has been closed for replies.
Best answer by MBake.4

In order to brake you need to apply torque in the opposite direction, current needs to flow out of the motor rather than in. The current regulators and svpwm will apply a voltage to the windings to achieve the desired current, in this case a negative iq.

To answer the actual question, when in the off phase of pwm the windings are essentially shorted, allowing the back-emf to produce a current through them. There is now energy stored in the magnetic field. When switching to the on phase, the current still wants to flow, and will produce the voltage necessary to flow back onto the dc bus.

Its kind of analogous to a boost converter, where the windings are the inductor.

2 replies

MM..1
Super User
November 15, 2021

You need for example AC DC step up converter for brake recharge.

MBake.4
MBake.4Best answer
Associate
November 21, 2021

In order to brake you need to apply torque in the opposite direction, current needs to flow out of the motor rather than in. The current regulators and svpwm will apply a voltage to the windings to achieve the desired current, in this case a negative iq.

To answer the actual question, when in the off phase of pwm the windings are essentially shorted, allowing the back-emf to produce a current through them. There is now energy stored in the magnetic field. When switching to the on phase, the current still wants to flow, and will produce the voltage necessary to flow back onto the dc bus.

Its kind of analogous to a boost converter, where the windings are the inductor.