Here are my issues:When I create a new project and press "Generate", CubeMX gets stuck and does nothing.When I try to open any of the demo projects and press "Update", CubeMX also gets stuck and does nothingThis is using ST Motor Control Workbench 5....
This is the monitor from the legacy workbench. Whenever I try to set a speed and press "Start Motor", it immediately drops to 0. Also, the status is permanently set to "stop".This image is of the motor pilot v 5.Y.3