STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1735 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4881 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9582 Views
  • 5 replies
  • 3 kudos

B-G431B-ESC1 Firmware Performance and De-sync Issues

I'm trying to create an esc for a drone using the B-G431B-ESC1. Our project requires that we use open source firmware so I'm using the STMCW firmware, and the motor profiler tool. I am comparing results to another ST-based esc that runs BLHeli firmwa...

SStee.1 by Associate
  • 1795 Views
  • 2 replies
  • 0 kudos

EVALSPINN32F0H60 on STM32CubeIDE

We are trying to evaluate the EVSPIN32F0602S1 motor driver. I've found I should use the 6 step driver firmware project EVALSTSPIN32F0H60 for this, but it turns out by default only IAR and Keil uVision are supported which we don't have. We work with S...

BHari.1 by Associate
  • 1150 Views
  • 1 replies
  • 0 kudos

EVALSPINN32F0H60 on STM32CubeIDE

We are trying to evaluate the EVSPIN32F0602S1 motor driver. I've found I should use the 6 step driver firmware project EVALSTSPIN32F0H60 for this, but it turns out by default only IAR and Keil uVision are supported which we don't have. We work with S...

Luuk1 by Associate II
  • 3207 Views
  • 4 replies
  • 0 kudos

Motor not spinning

Hey guys,:eyes: I'm trying to drive a 3kw brushless motor using HALL sensors with a single shunt custom board, based on the stm32f103rb(LQFP64) with the following configuration:MCSDK_v5.4.7-FULLMCU: STM32F101RB, 72MHz, Ext ClockMotor parameters:24 po...

0693W00000Y8FvTQAV.png 0693W00000Y8IUVQA3.png
MOhir.1 by Associate
  • 1729 Views
  • 1 replies
  • 0 kudos

Erasing memory corresponding to segment 0: Erasing internal memory sectors [0 29] Error: failed to erase memory

Error: failed to erase memoryEncountered Error when opening C:\ST\STM32CubeIDE_1.11.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.500.202209151145\tools\bin\STM32_Programmer_CLI.exeError in STM32CubeProgrammer...

0693W00000Y8I1EQAV.png

I need to develop a controller for 2 Wheeler BLDC PMSM Hub Motor - 350W, 48V, with Hall sensor feedback.. Please suggest ST existing solutions - Development board + Firmware using which I can test performance on my 2 wheeler.

Plan is to use existing development boards from ST and test on 2 wheeler. Once performace is validated, we will modify the hardware and also develop additional peripheral firmware.Looking for both 6 STEP solution and also FOC.Regards,Anil