cancel
Showing results for 
Search instead for 
Did you mean: 

How can we use LwM2M anjay SDK with STM32F4xx series? Is there an example with STM32F4xx?

VGoya
Associate II
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

The Embedded Partner Website of AVSystem says about Anjay LwM2M SDK: 

Anjay is an LwM2M SDK that enables the LwM2M protocol on any hardware device. It features a completely internal implementation of CoAP and is able to run on any kind of platform. The product is released as an open-source and available at: https://github.com/AVSystem/Anjay.

Commercial options which include support and advanced features are also available as a terminator T800.

Probably only AVSystem will be able to help you and tailor the package to a specific target platform.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

The Embedded Partner Website of AVSystem says about Anjay LwM2M SDK: 

Anjay is an LwM2M SDK that enables the LwM2M protocol on any hardware device. It features a completely internal implementation of CoAP and is able to run on any kind of platform. The product is released as an open-source and available at: https://github.com/AVSystem/Anjay.

Commercial options which include support and advanced features are also available as a terminator T800.

Probably only AVSystem will be able to help you and tailor the package to a specific target platform.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
VGoya
Associate II

Hi Peter,

Thanks you so much..

Please help us on below mention queries:-

Can you please share a link of terminator T800?

Can we interface LwM2M SDK with bare metal device or it required RTOS?

What are the minimum device configuration(Flash size, RAM size, GPIOs etc.) required for LwM2M SDK

Thanks

Vijendra

Peter BENSCH
ST Employee

Please direct your questions to AVSystem, who will be sure to answer them to your satisfaction.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.