cancel
Showing results for 
Search instead for 
Did you mean: 

how to tell my motor's max. rpm ?

dannypkchan
Associate II

if I keep increase the speed_value, my little motor spin very fast all of of sudden stop, I think it's caused by IsSpeedReliable or other FAULTs

is there any variable that I can closely monitor before motor reached its limit ?

MC_ProgramSpeedRampMotor1(speed_value, 10);

thanks,

Danny

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Laurent Ca...
Lead II

Dear @Community member​ 

Welcome to the STM32 Community

Could you give more details to the STM32 Community about your setup -the material you use- ?

(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)

And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?

And eventually more details about your application...

Best regards

dannypkchan
Associate II

Hi Laurent,

SW : MotorControl Workbench 5.Y.3

SW : Motor Profiler 5.Y.3

HW : B-G431B-ESC1

I use generated code from CubeMX, my question is if how can I tell from software side I already reached the MOTOR limit ?

thanks,

Danny