User Activity

The motor will stall at lower RPM,We found that the MCU did not detect a high current pull before the rotor stalled.Stop the motor because of MC_LF_TIMER_FAILURE (RUN_STAY_WHILE_STALL_MS set to 2000, should be enough),Is there any parameter that can ...
Step 1I have a motorUse EVB-F302+iHM08M1 to get motor parameters through Motor profiler as follows. Step 2I need to use EVB-STEVAL-SPIN3202 of STSPIN32F0A,execute Six-Step Sensorless Example code,STEVAL-SPIN3202\Demonstration\6S_STEVAL3202_SL_VM.stmc...
For example current detection, HW:STEVAL-PTOOL2V1SW:en.stsw-ptool2v1_v1.0.0.zipIt will be abnormal when it is about 4A or below, and it cannot read below 1A.About 4A or more (to more than 10A) can be detected normally,Could you please help me where m...
Hello, I am a newcomer and want to ask a newbie questionI researched EVB-EVSPIN32G4 and found that there is no example of this.Both Demostrations need list EVB profile. So I can't directly operate them.1. ST Motor profiler2. MC WorkbenchWhat time doe...
Posted on May 18, 2015 at 03:46STM32Cube 3v1.1.1 USB issue I use same operator to genertor  example code of USB HID/CDC...etc. on different HW baord.1. STM32F303VC for STM32F3DISCOVERY 2. STM32F302CC for My target board DISCOVERY is okay, my target ...
Kudos from