Skip to main content
Associate II
January 20, 2024
Question

How to controll esc with pwm signal from RC controller

  • January 20, 2024
  • 8 replies
  • 4296 views

So i have this simple code for pwm input for the rc controller :

void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef* htim)
{
if (htim->Instance == TIM2)
{
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1)
{
capture_value[0] = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_1);
if (capture_value[0])
{
frequency[0] = SystemCoreClock / capture_value[0];
duty_cycle[0] = 10000 * HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_2) / capture_value[0];
}

} }

How to take the value of  capture_value and controll an ESC with it?  i feel like i tried anything at this point and it just wont work. Here is my last attempt 

uint32_t mappedValue[0];
uint32_t pwmInput[0];

long map(long x, long in_min, long in_max, long out_min, long out_max)
{
return (x - in_min) * (out_max - out_min + 1) / (in_max - in_min + 1) + out_min;
}

// Function to set PWM duty cycle for motors
void setMotorPWM(uint32_t motorIndex, uint32_t pwmValue)
{
// Ensure motorIndex is within bounds
if (motorIndex < 4)
{
// Set PWM duty cycle for the corresponding motor channel
if (motorIndex == 0)
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_1, pwmValue);
else if (motorIndex == 1)
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_2, pwmValue);
else if (motorIndex == 2)
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_3, pwmValue);
else if (motorIndex == 3)
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_4, pwmValue);

// Optionally, update the duty_cycle array
duty_cycle[motorIndex] = pwmValue;
}
}


void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
// Assuming this callback is triggered based on the PWM input from the RC controller
if (htim == &htim1)
{
// Read the PWM input value from your RC controller (you need to implement this part)
pwmInput[0] = duty_cycle[0];

// Map the PWM input to the desired range for your motors
mappedValue[0] = map(pwmInput[0], 0, 2000, 50, 150);

// Set the PWM duty cycle for the first motor
setMotorPWM(0, mappedValue[0]);
}
}

------------

int main(void)
{
/* USER CODE BEGIN 1 */
// Initialize your hardware peripherals (TIM, GPIO, etc.) and system

// Start PWM for all motor channels
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_2);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_3);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_4);

 

 

EDIT: I am using STM32F07G - disc1

This topic has been closed for replies.

8 replies

waclawek.jan
Super User
January 21, 2024

> i tried anything at this point and it just wont work

What is "just wont work"? What are the expectations and what is the observed behaviour? Are the interrupts occuring?

JW

MatyášAuthor
Associate II
January 21, 2024

When i tried to controll the esc potenciometer

uint16_t ADC_Data=0;
int ADC_Converted = 0;
volatile uint32_t myVariable = 0;


long map(long x, long in_min, long in_max, long out_min, long out_max)
{
return (x - in_min)*(out_max - out_min + 1) / (in_max - in_min + 1 )+ out_min;
}

void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
ADC_Converted = map(ADC_Data, 0, 2000, 50, 150);

TIM1->CCR1 = ADC_Converted;
}

the esc calibrates and starts working completely fine, but when i try to use the previous code, the esc isn working at all

@waclawek.jan 

cedric H
ST Technical Moderator
January 22, 2024

Hello @Matyáš ,

Why two posts for the same question ?

Did you look at the answer I did to your initial post here.

Regards

Cedric

MatyášAuthor
Associate II
January 22, 2024

Hello @cedric H 

Sorry , you said I put my question to the wrong section so i wanted to delte the previous but couldnt.

Anyway I downloaded the program, but I couldnt find my STM32F407G-disc1 there. Does that mean it doesnt have any motor controll unit?

Thank you for your time.

Matyáš