STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1742 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4891 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9592 Views
  • 5 replies
  • 3 kudos

FOC SDK: maximum rotation speed limited

Posted on July 03, 2014 at 08:16We are using the FOC SDK 4.0, the eval board STEVAL-IHM039V1 (STM32F415ZG) and a 400 V, 1kV motor driver STEVAL-IHM025V1.The motor is working with no mechanical load and a quadrature encoder as position feedback. Cont...

Using VREFBUF for motor control

Hey everyone,the STM32G4s (including the STSPING4) have the VREFBUF feature, which allows to use an embedded voltage reference as reference voltage for the ADCs and DACs.I’m a bit surprised to see, that this is not used by default on the official dev...

dfrejek by Associate III
  • 981 Views
  • 0 replies
  • 0 kudos

where to find the define data

Hello,Now I am refer to a design of NUCLEO-G474RE board for Motor Control with 6 step method. I found there are some define data of TIM setting. but I cannot get the value of the define data. could you tell me where to find the defined data?Thanks!dq...

dqsh06_0-1721643468493.png dqsh06_1-1721643520966.png
dqsh06 by Senior
  • 2795 Views
  • 5 replies
  • 0 kudos

Motor Pilot and Plot

Hi,I'm using MC WB 6.3.0 with Motor Pilot.I wonder how to plot the following signals that are defined in MC WB in Motor Pilot:PWM_CHU_H, PWM_CHV_H, PWM_CHV_H,BEMF_U, BEMF_V, BEMF_W  I don't see these registers are defined in the list of Registers in ...

Texram_0-1721086176101.png
Texram by Associate III
  • 2130 Views
  • 2 replies
  • 0 kudos