STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1816 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4956 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9713 Views
  • 5 replies
  • 3 kudos

B-G431B-ESC1 not connecting to Motor Pilot

I have crated a start project for the B-G431B-ESC1 using MC Workbench 6.3.0I used the following settings:Motor 'Bull Running BR2804-1700kV' and Inverter 'B-G431B-ESC1' the project User Interface show ON for 'Over USART A' at 115200 baud.I can build c...

murpia by Associate II
  • 2687 Views
  • 5 replies
  • 1 kudos

DRV8323 driver with STM32

Hi, has anyone been able to successfully interface the DRV8323HRTAR with an STM32? I have been using an STM32F072RB, and have been trying to use ST's motor control workbench to generate code for controlling a BLDC motor. I've used the .ioc generated ...

TomLillie by Associate II
  • 1994 Views
  • 0 replies
  • 0 kudos

BLDC motor control with STM32 G071RB

Hi,I want to control BLDC motor with X-IHM07M1 motor driver and stm32 nucleo-G071RB microprocessor. I had read that this motor driver is compatible with Nucleo boards, but when I entered the Motor Control Workbench application, it only highlighted ce...

Batuhan35 by Associate II
  • 1499 Views
  • 0 replies
  • 1 kudos

Duty cycle control or phase shifting

I want to control a TRIAC's gate which will be working on 230V AC. I managed to create a one-pulse PWM based on zero-crossing detection. I want to implement a soft start function. To do that, I implemented soft start by controlling the duty cycle. Ho...

xXczachaXx_0-1722015818088.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.