STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to send data from Windows to HID keyboard?

Hello everyone! It's may be not the good place to state this problem but I am trying for days to send data from Windows to my STM32F103C8T6 CustomHID keyboard with Visual Studio in c#.I tried many libraries and stuffs that did not work. Like this one...

HGaut.1 by Associate II
  • 2307 Views
  • 2 replies
  • 1 kudos

Debug the code through uart

Hi!I am using STM32F373RCT6 controller on custom board. In that board we have used USB to serial convertere chip FT2232HL-REEL and it is connected to USART1 (PA9 and PA10). STM32F373RCT6 system clock frequency is 70MHz.Can I use USB to serial option...

GAGGA.1 by Associate II
  • 8539 Views
  • 6 replies
  • 0 kudos

Resolved! VDDSDMMC AND VDDUSB Clarficiation

SO i was doing some stm32 research and developed some application now i am going in production phase. Now i wanted to use stm32f765 but there are couple of variants in that series.I am getting confused between this two models STM32F765ZIT6 and STM32F...

Resolved! How to use lwip library with RTOS?

Hello every one; I would like to use lwip with RTOS( In DHCP Mode ). I try use lwip without RTOS ( In DHCP Mode ). It's work but I use lwip with RTOS is not work. I confuse to set priority (NVIC according to FREE RTOS ) lwip with RTOS. Could you plea...

0693W000004K7ikQAC.png 0693W000004K7ifQAC.png 0693W000004K7iaQAC.png 0693W000004K7iuQAC.png
Gz by Senior
  • 1244 Views
  • 1 replies
  • 0 kudos

Motion MC Library use?

Hi everyone, It seems I'm always coming across this issue in one form or another. I want to link in the "libPDMFilter_CM4_GCC_wc32.a" St Motion Library, and I'm entering the library name and path in the linker/Libraries section.I have included an ima...

kvresto by Senior
  • 2088 Views
  • 1 replies
  • 0 kudos

About Mass Storage

Hi, all.​I am making a USB MASS STORAGE program.It is recognized by Windows10 and can be used as a drive after formatting.I was able to copy the file and open it correctly.However, when I reset the NUCLEO board, windows prompts me to format it again....

Goemon by Associate II
  • 2058 Views
  • 4 replies
  • 0 kudos