2019-09-27 4:43 AM
Hello USB HID gurus !
How I can send on IN endpoint 0x81 for HID Custom Descriptor with HAL ?
I use USBD_CUSTOM_HID_SendReport
and endpoint is 0x81 until
#define EP_ADDR_MSK 0xFUI can see my report data on USB Bus Analyzer at OUT EP 0x1 and not on IN EP 0x81
function call is with ep_addr = 0x81 but with mask we get 0x1
But application is listening at /dev/hidraw1 at IN EP 0x81
see line 20
/**
* @brief Send an amount of data
* @param hpcd PCD handle
* @param ep_addr endpoint address
* @param pBuf pointer to the transmission buffer
* @param len amount of data to be sent
* @retval HAL status
*/
HAL_StatusTypeDef HAL_PCD_EP_Transmit(PCD_HandleTypeDef *hpcd, uint8_t ep_addr, uint8_t *pBuf, uint32_t len)
{
PCD_EPTypeDef *ep;
ep = &hpcd->IN_ep[ep_addr & EP_ADDR_MSK];
/*setup and start the Xfer */
ep->xfer_buff = pBuf;
ep->xfer_len = len;
ep->xfer_count = 0U;
ep->is_in = 1U;
ep->num = ep_addr & EP_ADDR_MSK;
if (hpcd->Init.dma_enable == 1U)
{
ep->dma_addr = (uint32_t)pBuf;
}
if ((ep_addr & EP_ADDR_MSK) == 0U)
{
(void)USB_EP0StartXfer(hpcd->Instance, ep, (uint8_t)hpcd->Init.dma_enable);
}
else
{
(void)USB_EPStartXfer(hpcd->Instance, ep, (uint8_t)hpcd->Init.dma_enable);
}
return HAL_OK;
}Changing mask to 0xFF enumeration fails; descriptor exchange should run on OUT EP 0x1 and not on 0x81
Any one using HID custom with success on /dev/hidraw1 in linux ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.