STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 can't create second FreeRTOS task.

Hi,I'm using STM32H745 and CM4 core runs with RTOS. I am not able to create the second task because xtaskcreate() does not return pdPASS. It seems like it can't allocate enough memory. I tried to create 2 tasks with stack depth equal to 1024. If I re...

Frak.1 by Associate II
  • 3391 Views
  • 7 replies
  • 0 kudos

Basic data transfer with USB CDC (FS) between PC and the Nucleo-F411RE board does not work. Please help me!

I would like to send data from the Nucleo Board F401RE or F411RE to the PC via the USB interface. The data should be transmitted via a virtual COM port (CDC protocol) with Full Speed (FS). Unfortunately this does not work! For testing I use also a Nu...

MScha.1 by Associate II
  • 2552 Views
  • 1 replies
  • 0 kudos

program STM32f103c8t6 with USB cable

hi thereI just bought a stm32f103c8t6 bluepill board. I was wondering if I can load the codes using the USB port. I watched this videohttps://www.youtube.com/watch?v=fD1Bzf2iP_E&list=UU_0GzDTV2G3m2Pi4gD2nTiQ&index=73but I want to use Keil for loading...

Ala by Senior
  • 827 Views
  • 0 replies
  • 0 kudos

Resolved! Ethernet configuration of MAC address

Hi everyone,I'm configuring the Ethernet MAC address over CubeMX for a NUCLEO-F746ZG target. Default address is 00-80-e1-00-00-00 which identifies ST manufacturers.I was wondering if I can freely manipulate the other 24 bits for an industrial purpos...

Nadreoh by Associate III
  • 5391 Views
  • 3 replies
  • 0 kudos

Is the modifications in the .c files and .h files of STL library (en.x-cube-classb-v2-3-0) is allowed?

Hi,We integrated en.x-cube-classb-v2-3-0 package in my application. Which is actually failing in runtime CRC test. I reduced the block size, which is actually 64 and I changed to 4  #define STEPS_NUMBER     ((uint32_t)ROM_SIZE/4u) and added some co...

Anitha by Associate III
  • 828 Views
  • 0 replies
  • 0 kudos