Skip to main content
ECarm.1
Visitor II
February 3, 2020
Question

Problems entering bootloader mode on STM32F072 with readout protection level 1.

  • February 3, 2020
  • 0 replies
  • 536 views

I'm developing firmware update for an application based on a STM32F072, using the built-in bootloader via UART1.

The method to enter bootloader is jump to Bootloader addres (as found on ST community discussions).

I managed to get Bootloader commands working with readout protection level 0 (for debugging); after setting RDP to level 1, the STM32 seems not to enter Bootloader mode any more: it seems being stuck in the loop waiting for boot interface selection, as I get no answer (neither 0x79 nor 0x1f) when sending 0x7f pattern on UART1 (user application not starting also).

Thanks in advance for any help.

This topic has been closed for replies.